SAFEPARAM.SIN.DISTINCTPULSE
Description
This setting indicates whether pulses on safe inputs must all be distinct from each other (i.e., offset from each other or different periods).
This does not disable the check for pulses on safe inputs. It only allows or disallows having the same pulse signal across safe inputs. |
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
02-01-02-000 |
|
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 (Disabled) or 1 (Enabled) |
Default Value |
0 (Disabled) |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
SAFEPARAM.SIN.DISTINCTPULSE |
3101h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |